REMINDER: Our logistics will close on Tuesday 19/01/2012

holiday schedule

REMINDER: Our logistics will close from January 19th to 29th for the Chinese New Year. No parcels will ship during that time period. Everything will back to normal since January 30th.

 

Happy Chinese New Year!

Post to Twitter Post to Facebook

New Product Post

We are going to set up an indoor air quality monitoring system. And this Grove - air quality sensor is just in time. This one is a multifunctional one, and you can keep alcohol, carbon monoxide, acetone, thinner, formaldehyde and other slightly toxic gases under control with this all-in-one sensor.

Car stays one of the hottest topics among people. However hacks on car get trapped by power somehow. That’s why we prepare this high current CPT-C5 power converter 12V/24V switch to 5V. The output current can be high up to 5A! Now nothing can stop you from power up a real project in a car!

And next, we have this light and convenient 13.56MHz RFID book tag. Use it like a sticker, and post it upon anywhere that you would love to make some identification, for example, books, goods and something else. To make a whole solution, you will also need a RFID reader, such as NFC Smart Card Reader that fulfills the read-and-write function. And the last, we have Probe jumper wire – 8pcs at hand. We can’t store much cables because needs for different cables keep popping up. So here we have another kind of cable with two probes on each side. Find it useful? Just stock some on your table.

Post to Twitter Post to Facebook

Spring Festival Party

Spring Festival is coming around the corner. To celebrate it, we hosted a Spring Festival party. Everyone was asked to prepare a hat, so here we have these lovely photo shots:

Time flies. But it looks like someone can shake faster than time!

This hat was made of spare wall paper, totally green. That’s why it won the energy-saving award.

Laser cutting machine is versatile. It can not only make you a project box, it can make you an elegant little hat.

Enjoy the party! Best wishes for all of you.

Post to Twitter Post to Facebook

New Product Post

Spring Festival is fastening up its pace. Only two weeks away the biggest festival for Chinese people is waiting. Everyone is busy imagining pictures of celebration, or worrying about how to get a back-home train ticket(that’s kind of a flight, believe me, but all the trouble will just add on the joy when they finally get home).  Back to our business, this week we bring you some DFrobot products and improved RF kits.

First, let’s check out two updated RF kits: Grove – 433MHz Simple RF link kit and Grove – 315MHz Simple RF link kit.  These boards are revised from our older products: 433Mhz RF link kit and 315Mhz RF link kit. We decided to make them more user-friendly, so Grove connector was added to remove any soldering work that might needed. But two visions are functionally identical, so more choice~

And next on, we have two boards catering for robot fans: Romeo-All in one Controller and 2A Motor Shield For Arduino. We get them from DFrobot — a Beijing based robot-centered OSH store. They do pretty good job on creating some boards and tools for robot. If you are working on a robot-related project, check these useful boards.

Final but not the least, we have Grove – Infrared Temperature Sensor. There are many solutions to detect temperature. Thermistor definitly costs the least. But, not satisfied with now accuracy and feel like to improve it? Try infrared temperature tech.

OK, then hope all of my friends survive this crazy ticket season…

Post to Twitter Post to Facebook

New Product Post

The last day of 2011, and the eve of 2012, people in my communities keep talking about their bucket lists continuously and continuously. You are pushing my back to hurry up, right? OK, OK, then a big New Product Post seems necessary now.

First, let’s check some gadgets that might smooth your working:

On the left is 38-In-1 Interchangeable precise manual tool set JK-6088. Kits always come with some specific screwdrivers or wrenches to help you assemble the kits. However, sometime after you finish the kits, tools like those usually can’t be found anymore. That’s the moment you really realize the convenience  a whole package tool can bring to you.

In the middle we have Sealed Membrane 3×4 button pad with sticker. We have once sold a similar one, and found a slimmer version. Does this one match your need?

And the right is Solder Assist Kit. It consists of knife, fork, reamer, magnifying glass(5 times)and some other things like that. It’s designed to improve your precision and efficiency of soldering.

Wow, next coming up are a series of solenoids. We have received some letters asking us to prepare some solenoids. Then by a shopping of local electronic market, we have found a number of solenoids in different specs.

Solenoid is a kind of transducer device that can convert energy into linear motion. Some people use it to create vending machine, protection circuit, music sets and so on. At the left upper corner is DC framework miniature solenoid VL-0063, 14.8V. The one beneath it is DC framework solenoid HCNE1-0416, a 24V DC One-way self-holding solenoid. At the left down corner is DC One-way self-holding solenoid HCNE1-B1031D, 24V and recommended by our engineers. At the right down corner shows DC framework solenoid HCNE1-0520. With 12V low voltage requirement, it’s more suitable for small or handy projects. Another 24V solenoid is DC framework solenoid HCNE1-0630 at the upper right scorner. Above are all kinds of solenoids we presented last week. Looking for something that move forth and back? Try them out~

Next coming is one new member in our grove family–Dust Sensor. Discussions about air quality get hotter and hotter these days. PM2.5 and PM10 appear almost every 3 days on newspaper. Compared to traditional dust sensor, this one has a more accurate output and higher sensitivity.

And finally, welcome another expansion of Gadgeteer! This time what are added is LED7R module, USB client SP module, Music module, CAN DW module, Bluetooth module, Motor Driver L298, and Xbee module.


Post to Twitter Post to Facebook

Happy New Year 2012!

Happy new year2

New Year’s Holidays from January 1st to January 3rd. Seeed Studio’s online store is taking orders as usual on holidays! All packages will ship on Tuesday January 3rd, 2012.

 

Gift Certificates are always available.

Post to Twitter Post to Facebook

Get Adobe Flash playerPlugin by wpburn.com wordpress themes